AnsweredAssumed Answered

Multiple 34970A & BL3, not starting all DAQ at once

Question asked by ryaninlouisville on Nov 28, 2011
Latest reply on Dec 1, 2011 by ryaninlouisville

I am running BL3 under Win 7 32 bit. I have 2 34970A's communicating on GPIB.

 

I can start both of them scanning with the run all button several times, but after a while only the first DAQ will start and scan.  When I try to stop them, one of them stops but the other one still has the running box there in BL. If I click on that, I get the message "MSG_STOPPING_UNDER_PROGRES".  The only way to stop this issue it is to shut down BL and restart it.  Then it will work fine for a few times, then start acting up again.

 

Any ideas?

 

Thanks,

 

Ryan

 

Edit: 34970 was 34972  

Outcomes