Is there a command to the determine the serial number of a 33120A? When I use the *IDN? command I believe Field 3 should be the serial number, but the result is zero. If anyone can help thanks.
Unfortunately the serial number is not stored anywhere inside the function generator. That 0 is where it would be, but they ran out of memory and this thing was designed when memory was hard to come by.
JoeD