AnsweredAssumed Answered

Setting up Clustered SC-FDMA measurement in 89601B (with BHG license)

Question asked by sartaj on Jul 6, 2012
Latest reply on Jul 16, 2012 by DaveHornbeck
I need to know what all parameters need to be set for a clustered sc-fdma measurement for LTE-Advanced FDD. The resource allocator used for LTE-Advanced is the same as LTE and does not contain anything specific to setting up the two clusters for each slot. The auto-mode fails to syn when a LTE-Advanced signal is feeded in to the analyser. the help says that it is capable of demodulation clustered SC-FDMA. Also, does the size of the two clusters need to be same in each slot (number of resource blocks allocated be same)?  

Outcomes