I am trying to install the E4438C ESG Intuilink software onto a Windows7 PC. I keep getting an error relating to IO Library files. Has anyone used the ESG Intuilink successfully on a Win7 PC?
Can you verify the IO libraries version installed on your PC? It requires version 15.5 and above for it to work on the Win7. The current available IO libraries is version 16.1. Here’s the link:- http://www.home.agilent.com/agilent/pro ... indiosuite
If this doesn’t work after you have installed version 16.1, then it could be the Intuilink which not able to use on the Win7 OS platform.
Currently there is no further plan to enhance the Intuilink.
Can you verify the IO libraries version installed on your PC? It requires version 15.5 and above for it to work on the Win7. The current available IO libraries is version 16.1. Here’s the link:-
http://www.home.agilent.com/agilent/pro ... indiosuite
If this doesn’t work after you have installed version 16.1, then it could be the Intuilink which not able to use on the Win7 OS platform.
Currently there is no further plan to enhance the Intuilink.
Regards -