AnsweredAssumed Answered

6812B EXT SYNC

Question asked by kstemiller on Apr 11, 2011
Latest reply on Apr 15, 2011 by StevenLee
I need to generate a specific series of power interrupts. I have been able to get the output I want using the Trigger Control INIT:IMMED on the front panel. However I want to sync the interrupt to an external trigger. When I try to set up the TRIG:SOUR EXT I get no triggering. I have verified with a scope that that I see the internal pull-up and that I am able to ground it.  

Outcomes