AnsweredAssumed Answered

Class not registered Error

Question asked by shoemakesmusic on Apr 4, 2012
Latest reply on Apr 5, 2012 by shoemakesmusic
Hey guys, I am trying to run some of the example code that comes with the software for the 34401A.  I am running C# Example1.  When I run the project I get this error:

Retrieving the COM class factory for component with CLSID {FE9A1E9A-4294-4470-86
A2-08CBD637890B} failed due to the following error: 80040154 Class not registere
d (Exception from HRESULT: 0x80040154 (REGDB_E_CLASSNOTREG)).

Done - Press Enter to Exit


It sounds like I don't have something installed right.  I've checked my References in my project and it shows the Agilent34401Lib.  But maybe I am missing something else.  I have installed the IVI shared components and the Agilent drivers.  

Outcomes