Hello.
We have a ESG generator with IQ generation option.
I'm trying to upload IQ data files to the instrument using Signal Studio Toolkit.
When I try to connect to the instrument, the system succesfully initiate communication with GPIB, but after I press the button "FINISH" to finalize instrument configuration, something goes wrong, telling that intrument cannot be used.
I don't underdstand if it depends on instrument configuration, missing hardware/software options enabled, firmware bugs or whatever...
Please, could you clarify what are the minimum requirements on the instrument side to use the software?
Thanks
We have a ESG generator with IQ generation option.
I'm trying to upload IQ data files to the instrument using Signal Studio Toolkit.
When I try to connect to the instrument, the system succesfully initiate communication with GPIB, but after I press the button "FINISH" to finalize instrument configuration, something goes wrong, telling that intrument cannot be used.
I don't underdstand if it depends on instrument configuration, missing hardware/software options enabled, firmware bugs or whatever...
Please, could you clarify what are the minimum requirements on the instrument side to use the software?
Thanks
The minimum Hardware requirement for the ESG when used with the N7622A Signal Studio Toolkit:
Model Number – E4438C
Firmware revision – C.04.10 or later
Option 601 or 602 installed.
Regards -