Hello all,
I am performing a S-parameter simulation that needs to switch between 8-states. I have 8 variables which control which state the system is in, i.e. if var1 = 1, the system is in state 1. For each state I need to perform a frequency sweep. At the moment I am performing the frequency sweep for each state separately by manually toggling each of the 8 variables and then running the simulation. Is there a way of automating this process and plotting the S21 of each state on a single graph? i.e. set var1=1, all others=0, perform sweep, set var2=1, all others=0, perform sweep etc.
Thanks in advance for your help.
I am performing a S-parameter simulation that needs to switch between 8-states. I have 8 variables which control which state the system is in, i.e. if var1 = 1, the system is in state 1. For each state I need to perform a frequency sweep. At the moment I am performing the frequency sweep for each state separately by manually toggling each of the 8 variables and then running the simulation. Is there a way of automating this process and plotting the S21 of each state on a single graph? i.e. set var1=1, all others=0, perform sweep, set var2=1, all others=0, perform sweep etc.
Thanks in advance for your help.
have fun with RF
Henry