AnsweredAssumed Answered

34972A cannot get DHCP address

Question asked by mattski on Jul 13, 2011
Latest reply on Sep 20, 2012 by mario1980
I have a 34972A which I'm trying to hook up to our LAN.  I have verified connectivity of the network port and cable (which is on a hub) by checking that a computer is able to connect to the network.  When I put the instrument on this port it is not able to get an IP address and eventually it will auto-configure a 169.254.x.x address.

Any suggestions to get this connected?  

Outcomes