AnsweredAssumed Answered

E4438C Triggering

Question asked by sndman99 on Dec 2, 2011
Latest reply on Dec 8, 2011 by tabbott
I am using an ESG E4438C and was wondering if there is a way to have the system transmit when traffic is detected on an ext input?  I have used list files before for similar projects but it is labor intensive to correlate amplitude settings in a list to correlate to the traffic  on the ext input. Was hoping there was a setting that would detect voltage change on the external input to trigger the transmit.

Ideas?

Thanks
Sandy  

Outcomes