We just received our new Agilent 33522A Function Generator. But i am missing the Waveform Editor Software promissed in the user guide.
"Agilent 33500 Series Product-Reference CD: This CD contains the 33500 Series instrument drivers, the Agilent Intuilink Waveform Editor software, the complete set of Agilent 33500 Series product manuals, and programming examples. The CD auto-starts and provides a Welcome page with instructions."
Where can i get the software? It isn't at the CD.
"Agilent 33500 Series Product-Reference CD: This CD contains the 33500 Series instrument drivers, the Agilent Intuilink Waveform Editor software, the complete set of Agilent 33500 Series product manuals, and programming examples. The CD auto-starts and provides a Welcome page with instructions."
Where can i get the software? It isn't at the CD.
Sorry for the promise, this was mistakenly put in to the manual. I am having the Agilent IntuiLink Waveform Editor reference removed ASAP.
The 33500 series was not actually designed to work with IntuiLink and is not supported for use with it. Agilent is currently working to develop the BenchLink Waveform Builder software package. This software will be designed for building and downloading arbitrary waveforms. A for pay version of the software will be released initially with a "lite" free version to follow.
In the mean time there are many other ways to create arbitrary waveforms. Two of my favorites are Matlab and Excel. There is an example program for using Matlab on this forum. If you would like to use IntuiLink you will not be able to directly send the waveforms to the instrument but instead you will have to save them as a CSV file which you can then transfer to your 3352xA via SCPI or USB thumb drive. To download the IntuiLink software please click the link below.
http://www.home.agilent.com/agilent/editorial.jspx?cc=US&lc=eng&ckey=1000000918:epsg:sud&nid=-536902257.536883183&id=1000000918:epsg:sud
Thanks,
Steve