AnsweredAssumed Answered

GPIB parsing error -1073807342

Question asked by samson41879 on Nov 9, 2011
Latest reply on Dec 14, 2011 by samson41879
Dear all...

I have a mysterious problem with visa32.DLL and GPIB communication with any Agilent instrument. In my case it is power supply, but it can be any instrument because error occures while opening a session with instrument.
I have two PCs - a first PC has Delphi 2005 installed with Agilent IO Suite 15.0, and a second PC has Delphi XE (2011) installed also with Agilent IO Suite 15.0.
I wrote the same application using Delphi 2005 and Delphi XE with the same visa32.DLL. On both of the Delphi versions compilations was successful, but only the
application that is compiled in Delphi 2005 is able to establish GPIB communication with an instrument on any other PC. The application writen in Delphi 2011 reports following
error: VI_ERROR_INV_RSRC_NAME (-1073807342) = The resources specified are invalid, Parsing error.

Does anyone knows what is the problem?

Thanks in advance!  

Outcomes