Good day!
The system worked on Laptop established by another man. Now I have another computer with no practice working with agilent.
The system is LCR meter - cryostat. Attached instruments: Agilent E4980A and scientific instruments model 9700. The system (windows xp) is running with NI MAX and Agilent VISA and with Agilent 8. The SI model 9700 is connected from RS232 via USB. The win system recognized it, the NI max recognized it, but at Agilent connection expert it all stopped by trying to send *IDN? to device (error timeout). When trying to run program vee it stopped saying error 811: resource found on this interface but not as ASRL4::INSTR.
Where can be a problem. I tryed different settings (changing primary - secondary VISA etc,) but nothing worked. I believe that there is just a small setting somewhere and everything will run.
Thank you for helping, Miro.
The system worked on Laptop established by another man. Now I have another computer with no practice working with agilent.
The system is LCR meter - cryostat. Attached instruments: Agilent E4980A and scientific instruments model 9700. The system (windows xp) is running with NI MAX and Agilent VISA and with Agilent 8. The SI model 9700 is connected from RS232 via USB. The win system recognized it, the NI max recognized it, but at Agilent connection expert it all stopped by trying to send *IDN? to device (error timeout). When trying to run program vee it stopped saying error 811: resource found on this interface but not as ASRL4::INSTR.
Where can be a problem. I tryed different settings (changing primary - secondary VISA etc,) but nothing worked. I believe that there is just a small setting somewhere and everything will run.
Thank you for helping, Miro.
In Agilent connection expert when trying to send command it takes very long to read it - cca 5 seconds - so the result is in time error of responding.
I must say, that I fresh install the system more than 10 times and because of unsuccess I tried to install things differently, for example usually be the first Agilent connection expert etc. So somewhere in the middle (around 5th attempt) the system worked. I was so excited and then try to install win 7 on another partition since it is needed to run other applications - but of course everything crashed. The problem is, that I dont know what I did actually. But I can tell, that not some special settings, it was mainly about primary VISAs.
My next question is, must be Agilent VISA primary, secondary or side by side.
The thing is that this device does not need to be check in Agilent connection expert via sending IDN.
In vee the following settings must be changed: In I/O - instrument manager - choose the device (ASRL1::INSTR in my case) then click settings and advanced. In direct I/O map change the end line - replace both n with r - THATS IT.
I hope that this will help to someone, Miro.