Hello, i just received my new 53220A, and i installed the updated version 16.1 suite that came with the package. I was previously running, version 15.1. Now the connection expert can not connect to any of my LAN instruments (i could connect to my 34410 with vr15.1). I can connect to the instruments by entering in the IP to web browser. Why can't Connection Expert see my LAN connected instruments?
Thanks
Thanks
Attachments
Is the DMM in the same IP address range (subnet) as your PC?
If its using Auto-Ip, I'd recommend rebooting the 34410A (give it like 2-2.5 minutes to stabilize the new connection).
The IP of the 34410A's i am trying to connect to are: 10.232.2.75 and 102322.61. My PC is 10.232.2.34, the subnet mask of all instruments and PC are the same. Does that help?
I tried a re-boot of instruments and my PC, no luck yet.
I tried another PC with older Suite version 15 (on the same network), and it found all instruments. I tried another PC with version 16 and that did not work.
1. go into Agilent Connection Expert
2. do a LAN search, let it finish completely
3. close Connection Expert
4. download the attachment and unzip the debug tool into an empty directory
5. double-click the .exe, and several logs will be output to that directory
6. zip up those files and email them to me at io-sw_support@agilent.com
Attachments
I have been running a LAN Auto find for about 30-40 minutes and it does not seem to finish?
It really shouldn't take more than a couple of minutes. I'd kill it and run the log tool.
I have sent you some log files to the e-mail you gave me.
This is the piece of code that does LAN device discovery using VXI-11 (your 53220 is newer, so it was picked up by our mDNS discovery algorithm). The engineer responsible for this code is out till Monday, so I'll have to wait till then to talk to him.
For the time being, I'd say you'll have to manually add the instrument address. Sorry for the inconvenience!
Cheers!
When using the 34410A internal web host, i connect through the browser and i can get access to a very nice front panel interface to control the instrument and take measurements/output data. Now when i connect to the 53220A i had that same expectation, however the only interface i see is to send commands and receive repose. Will the 53220A firmware be updated with a front panel interface/control through the web host (much like the 34410A) in the future?