Try to add it manually if aitosearch is not working with this usb-serial thing.
1. Open Vee 2. Open InstrumentManager 3. Righclick MyConfiguration and select "Add Instrument" 4. Interface Type: ASRL 5. Name: Whatever you want 6. BoardNumber: 1 7. Visa Alias: COM1 8. Visa Address: ASRL1::INSTR 9. Click OK
Go into the advanced settings on your instrument properties and verify the setup is correct (baud, read/write terminater, etc.). I may also help to have the Bus I/O monitor open so you can see what is sent over the IO.
1. Open Vee
2. Open InstrumentManager
3. Righclick MyConfiguration and select "Add Instrument"
4. Interface Type: ASRL
5. Name: Whatever you want
6. BoardNumber: 1
7. Visa Alias: COM1
8. Visa Address: ASRL1::INSTR
9. Click OK
Now test if its working...