Ok! Thank you! But I wanted to know if someone has already used, recommend or have another way to do this kind of check. I had seen this file and so I sent the message.
because VTEP is different hardware than Testjet - it requries special software/hardware to detect if VTEP is really functioning OK, not just simple measure as with testjet
this is why Agilent provides details on how to verify VTEP - and yes, many fixture houses already are using this equipment
only other way is to plug into a fixture on a test system
Yes, it is working fine. i.e. Fixture/programming house is using it to verify the VTEP and TestJet hardware.
http://www.home.agilent.com/agilent/editorial.jspx?cc=US&lc=eng&ckey=1923106&nid=-11143.0.00&id=1923106&pselect=SR.GENERAL
BR, Yang Hua