AnsweredAssumed Answered

MATLAB U3606A measurements

Question asked by baroskos on Jul 29, 2011
Latest reply on Aug 3, 2011 by lhornburg
I'm trying to record readings from my U3606A using MATLAB. So far I have been able to connect to the device by creating a VISA-USB connection and I am able to get the device to self test. I have tried fscanf to no avail.

I am also trying to change the voltage through the program. I'll start the instrument then connect to a simple circuit and send 1V through it. When I try to give the command "fprintf(obj,'Volt 2')" it changes the voltage to 0. It feels like progress since I am changing the output, but how do I get it to change to my specified value?

Any help with either one of these would be appreciated.  

Outcomes