AnsweredAssumed Answered

PNA-X sense2:noise:snp "NoiseParameter"

Question asked by jeffturp on Jun 21, 2013
Latest reply on Jun 24, 2013 by Dr_joel
I'm unable to save s2p file with "NoiseParameter". The command: sense2:noise:snp "NoiseParameter"
which is shown as an example in the SCPI help generates an error. The command: sense2:noise:snp:save "C:/Program Files/Agilent/Network Analyzer/Documents/MyNoiseParams.s2p", "NoiseParameter"
also generates an error. If the commands are used without the "NoiseParameter" argument everything works fine but of course no Noise Parameter data is saved.  

Outcomes