AnsweredAssumed Answered

vrf Merging Vee Programs from different sources: Reconcilin

Question asked by mark.goldberg on Apr 1, 2004
Joel,

If I follow you correctly you want to keep all the objects and just get rid
of the names in the instrument manager. If that is what you have in mind you
could setup all the boxes to have control inputs and drive them with an
array of the different parameters. That way if you ever have to run it on
the 1416 addy you could just add that to the inst mgr and change the
settings array. That way you can accommodate all the different
configurations and still only have one device in the inst mag.

Hope that was clear?

Mark

-----Original Message-----
From: DUNSMORE,JOEL (A-Sonoma,ex1) [mailto:joel_dunsmore@agilent.com]
Sent: Thursday, April 01, 2004 9:48 AM
To: VRF
Subject: [vrf] Merging Vee Programs from different sources: Reconciling
Direct IOs


Hi all,
     I'm trying to merge two different programs from two different
sources, which drive network analyzers.
In one program, it has two direct IO blocks, both GPIB 716, one labeled VNA,
one labled Network analyzer.

In the other program, I have 3 direct IO blocks, GPIB 716, one labeld PNA,
one PNA1 and one NetworkAnalyzer1.

Since all of these drive the same network analyzer, I want to get rid of all
but one.  I haven't been able to figure
out a way to do it, short of replacing them one at a time in each place they
occur in the program.  Any ideas? 

To make it more interesting, several of the ones labeled NetworkAnalyezer in
the IO manager have labeles in the VEE
program of PNA (@ 1416) which I assume because sometime in the past they
were hooked up with an NI card.

Thanks, Joel

---
You are currently subscribed to vrf as: Mark.Goldberg@ATK.COM
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes