AnsweredAssumed Answered

vrf VEE 6 Pro, Matlab and Vista

Question asked by VRFuser on Sep 27, 2008
Latest reply on Sep 27, 2008 by VRFuser
Hi all
I use VEE6 Pro on a XP desktop.  I recently purchased a Vista laptop on which VEE 6 installed ok and runs so long as there are no matlab functions used in the program. Unfortunately when my programs access the Matlab functions I get the following VEE Run Time error:

Could not start Matlab Script Engine (-3) Object title: MATLAB Script BUTTER Object Type: MATLAB Script Error Number: 591

I have no other versions of matlab installed on the laptop, as suggested in some of the archives.

I also get a whole lot of Registry Key Errors including:
Matlab.Aplication.single
Matlab.Aplication.singleCLSID
Matlab.Aplication.singleCLSIDCurVer
Matlab.Aplication.singleCLSIDNotInsertable
Matlab.Aplication.single.5
Matlab.Aplication.singleCLSID
Matlab.Aplication.singleNotInsertable
ect, etc, etc......
.....to the point of having to restart the laptop in order to stop the reigistry key errors popping up.

Has anyone else had the same experience?
Is this another of those "Vista issues"?
Does anyone know of a work around so that I can run my VEE6 programs for data processing on the vista laptop?

As always, thanks in advance
cheers
alex

PS: I searched the vrf archive and found one other reference to a similar issue with no replies....

From: Hynatec (oldenziel@hynatec.com)
Subj: [vrf] Vista and Matlab
Date: 2007-08-21 03:27:45
MID: 0000000054D9884439D2CE4AB325992309F09DE844E38B00
Atch: (No Attachments)

Hello,



I found out that Matlab scrips in VEE-Lab don't function in Windows Vista.

Is there any support?



Best regards,



Daniel Oldenziel

Regards
Alex

----------------------------------------------------------------
This message was sent using IMP, the Internet Messaging Program.


---
You are currently subscribed to vrf as: hua_jing@agilent.com To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive".
Search the Agilent vrf archive at "http://vee.engineering.agilent.com".

Outcomes