Hi,
How many 6032A units can be connected in parallel combination?
The operating manual (Sep. 2004) says (pp. 68) "Two units can be connected in an auto-parallel combination to provide twice the output current capability." but it also states earlier in the same section (pp. 67) that "Other configurations are possible.Contact Agilent Technologies, Power Products Division...", so I'm wondering if three units can be connected in an auto-parallel combination in order to provide thrice the output current.
Regards, Ramis.
How many 6032A units can be connected in parallel combination?
The operating manual (Sep. 2004) says (pp. 68) "Two units can be connected in an auto-parallel combination to provide twice the output current capability." but it also states earlier in the same section (pp. 67) that "Other configurations are possible.Contact Agilent Technologies, Power Products Division...", so I'm wondering if three units can be connected in an auto-parallel combination in order to provide thrice the output current.
Regards, Ramis.
I work for what used to be called the Power Products Division of Agilent many years ago, now called System Products Division.
I spoke with a few of my co-workers about your question here and we were wondering if you could give us an idea of what the load is going to be on the power supply. Is it resistive, inductive, or capacitive? Any details at all would be helpful.
Thanks!