I am using Visual Basic 6 and the SICL module to retrieve the data from a scan list on a 34970a. I use the ivscanf function but I can't seem to format the output to what I want. I need a comma-delimited string containing voltage measurements with double (preferable) or single precision values, not scientific notation. I know I can write a function to change the values but I would prefer to output right from the unit. I have tried lots of different combinations using the SICL manual as a guide but they all seem to be invalid.