<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.0 Transitional//EN"><HTML><HEAD><META http-equiv=Content-Type content="text/html; charset=iso-8859-2"><META content="MSHTML 6.00.2900.2668" name=GENERATOR></HEAD><BODY><DIV dir=ltr align=left><SPAN class=513120308-10082005><FONT face=Tahoma color=#0000ff size=2>Hi Dara,</FONT></SPAN></DIV><DIV dir=ltr align=left><SPAN class=513120308-10082005><FONT face=Tahoma color=#0000ff size=2></FONT></SPAN> </DIV><DIV dir=ltr align=left><SPAN class=513120308-10082005><FONT face=Tahoma color=#0000ff size=2>Thank you for the example. It operates smoothly, without any security changes while both accounts are identical. I think, I can proceed now to allow for unequal accounts. Once again, thanks.</FONT></SPAN></DIV><DIV dir=ltr align=left><SPAN class=513120308-10082005><FONT face=Tahoma color=#0000ff size=2></FONT></SPAN> </DIV><DIV dir=ltr align=left><SPAN class=513120308-10082005><FONT face=Tahoma color=#0000ff size=2>Best Regards,</FONT></SPAN></DIV><DIV dir=ltr align=left><SPAN class=513120308-10082005><FONT face=Tahoma color=#0000ff size=2>Frantisek</FONT></SPAN></DIV><BR><BLOCKQUOTE style="PADDING-LEFT: 5px; MARGIN-LEFT: 5px; BORDER-LEFT: #0000ff 2px solid; MARGIN-RIGHT: 0px"> <DIV class=OutlookMessageHeader lang=cs dir=ltr align=left> <HR tabIndex=-1> <FONT face=Tahoma size=2><B>From:</B> SARIASLANI,DARA (A-Sonoma,ex1) [mailto:dara_sariaslani@agilent.com] <BR><B>Sent:</B> Wednesday, August 10, 2005 2:30 AM<BR><B>To:</B> VRF<BR><B>Subject:</B> RE:[vrf] PNA Com Events<BR></FONT><BR></DIV> <DIV></DIV> <DIV dir=ltr align=left><FONT face=Arial color=#0000ff size=2><SPAN class=643280600-10082005>Hi Frantisek,</SPAN></FONT></DIV> <DIV dir=ltr align=left><FONT face=Arial color=#0000ff size=2><SPAN class=643280600-10082005></SPAN></FONT> </DIV> <DIV dir=ltr align=left><FONT face=Arial color=#0000ff size=2><SPAN class=643280600-10082005>Since we moved to WXP SP2 some security and DCOM settings were changed which explains why you may be having problems. Events can work with DCOM as well as COM and your PNA does not have to be on the same domain as your controller pc. You do however, have to set the proper permissions for DCOM thru the windows firewall on the PNA and anonymous access for DCOM on both the PNA and the client pc. If you go to the following site (<A href="http://na.tm.agilent.com/pna/xpsp2.html">http://na.tm.agilent.com/pna/xpsp2.html</A>), you will find instructions for setting up the permissions. There is a utility that is provided to simplify the setup on the PNA, but you must also manually perform steps 2-9 of the section "<STRONG><FONT face="Times New Roman" color=#000000 size=3>Settings to Allow Anonymous DCOM Access</FONT></STRONG>" on your client PC. If you also have a firewall on your PC, you may have to change some of its settings as well. The best thing to do is to turn your PC's firewall off (temporarily) and then try your program. if everything works, then turn it back on and try again. If it didn't work with the firewall turned on, then you must contact your IT support to configure the appropriate exceptions.</SPAN></FONT></DIV> <DIV dir=ltr align=left><FONT face=Arial color=#0000ff size=2><SPAN class=643280600-10082005>I have included a simple VEE program that works with Channel events when run inside or outside of a PNA.</SPAN></FONT></DIV> <DIV dir=ltr align=left><FONT face=Arial color=#0000ff size=2><SPAN class=643280600-10082005></SPAN></FONT> </DIV> <DIV dir=ltr align=left><FONT face=Arial color=#0000ff size=2><SPAN class=643280600-10082005>Best Regards,</SPAN></FONT></DIV> <DIV dir=ltr align=left><FONT face=Arial color=#0000ff size=2><SPAN class=643280600-10082005></SPAN></FONT> </DIV> <DIV dir=ltr align=left><FONT face=Arial color=#0000ff size=2><SPAN class=643280600-10082005>Dara Sariaslani</SPAN></FONT></DIV> <DIV dir=ltr align=left><FONT face=Arial color=#0000ff size=2><SPAN class=643280600-10082005>PNA Application Architect</SPAN></FONT></DIV> <DIV dir=ltr align=left><FONT face=Arial color=#0000ff size=2><SPAN class=643280600-10082005>Agilent Technologies</SPAN></FONT></DIV><BR> <DIV class=OutlookMessageHeader lang=en-us dir=ltr align=left> <HR tabIndex=-1> <FONT face=Tahoma size=2><B>From:</B> Hejsek Frantiek [mailto:fhejsek@cmi.cz] <BR><B>Sent:</B> Monday, August 08, 2005 5:46 AM<BR><B>Subject:</B> PNA Com Events<BR></FONT><BR></DIV> <DIV></DIV> <DIV><FONT face=Tahoma size=2><SPAN class=576151112-08082005>Hi All,</SPAN></FONT></DIV> <DIV><FONT face=Tahoma size=2><SPAN class=576151112-08082005></SPAN></FONT> </DIV> <DIV><FONT face=Tahoma size=2><SPAN class=576151112-08082005>Does anyone know how to communicate with Events in PNA DCOM on a remote computer? The DCOM itself operates smoothly but I am unable to use Events. PNA displays : "Member not found", see event log. Included vee file is an original Agilent example. In S</SPAN></FONT><FONT face=Tahoma size=2><SPAN class=576151112-08082005>et PNAOpen ... I have added the PNA name. I am using VEE 7.03 development and WXP.</SPAN></FONT></DIV> <DIV><FONT face=Tahoma size=2><SPAN class=576151112-08082005>Agilent says that the application must be run on the same computer to use events, but on a different place they claim that it is not needed (<A href="http://na.tm.agilent.com/pna/DCOMSecurity.html">http://na.tm.agilent.com/pna/DCOMSecurity.html</A>). I have tested access only from remote computer.</SPAN></FONT></DIV> <DIV><FONT face=Tahoma size=2><SPAN class=576151112-08082005>Both computers are in the same domain and even the same account doesn't solve the problem. My experiments with dcomcnfg only worsen the situation. I am not an expert and I haven't any idea how to continue. Thanks.</SPAN></FONT></DIV> <DIV><FONT face=Tahoma size=2><SPAN class=576151112-08082005></SPAN></FONT> </DIV> <DIV><FONT face=Tahoma size=2><SPAN class=576151112-08082005>Frantisek</SPAN></FONT></DIV> <DIV><FONT face=Tahoma size=1><FONT size=2><BR><FONT face=Tahoma size=1>--------------------------------------------------------------------------<BR>Frantisek Hejsek<BR>Microwave Measurement Laboratory (1013)<BR>Czech Metrology Institute<BR>Radiova 3, 102 00 Praha 10, Czech Republic<BR>E-mail: fhejsek@cmi.cz<BR>Tel: +(420) 266 020 172, Fax: +(420) 272 704 852<BR>-------------------------------------------------------------------------<BR><BR></FONT></DIV></FONT></FONT><BR>---<BR>You are currently subscribed to vrf as: fhejsek@cmi.cz<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list, email "vrf@agilent.com". <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com". </BLOCKQUOTE><BR>---<BR>You are currently subscribed to vrf as: rsb@soco.agilent.com<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list, email "vrf@agilent.com". <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".</BODY></HTML>
my prob is somewhat similar to David. Ifft
in matlab script takes time and built in Ifft function
does'nt return complex pairs. The delay might be becoz
of the matlab engine initialization .... but is there
any way to avoid that delay ...... by using compiled
function for example .........
____________________________________________________
Start your day with Yahoo! - make it your home page
http://www.yahoo.com/r/hs
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".