AnsweredAssumed Answered

vrf Hotkey Troubles

Question asked by VRFuser on Jun 26, 2005
Hi Shawn -

what would you use for the key tracing?

Removing software isn't that simple either because of the amount of
software
involved.

I could start with the antivirus software since that is always a good
bet
but sadly IT will shut down my PC if I don't have AV software running so
this
a bit of a problem.. no PC, no Vee testing

S.

> -----Original Message-----
> From: Shawn Fessenden [mailto:shawn@testech-ltd.com]
> Sent: 27 June 2005 13:45
> To: SPANGENBERG,SASCHA (A-Scotland,ex1); PDL-LISTS,VRF (A-Lists,unix1)
> Subject: RE: [vrf] Hotkey Troubles
>
> > does anyone have problems with
> > hotkeys not working properly in
> > vee 7.0?
>
> No I don't have any problems, but considering all the
> comments it *is* kind of strange. Sometimes Ctrl-v doesn't
> work, but that's only because I forgot to press Ctrl-c in the
> first place
>
> All my hardware is rather old and slow too. The computers
> aren't exactly running stripped down configurations, but I
> don't run any anti-virus software, firewall software, popup
> blockers, ad-watch or anything like that.
>
> If you really want to get to the bottom of it, you could
> trace key messages through the system and find out exactly
> what it is that's eating them but it might be easier to just
> experiment with yanking stuff out to see what's causing the problem.
> -SHAWN-
>

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes