AnsweredAssumed Answered

vrf VEE and Suite 14 IO Libraries Installation problem/ w2k versus X P / IOSuite14.1 Bug ?

Question asked by VRFuser on Nov 21, 2005
Dear Denis,

Agilent does have recommendations on how to operate a mixed system i.e. Agilent and another VISA. I'm no expert on this by any stretch of the imagination but you may find the following useful.

Did you install NI VISA first? Agilent's IO Libraries Suite has some specific technologies that make it work well with NI-VISA and NI-488.2.  If you install NI-VISA first, Agilent's installer can do a good job of discovering the NI software it must work with and can install the right components in the right places. 

This is because Agilent VEE Pro supports both the SICL and 488.2 I/O API's for searching for GPIB interfaces.  The Agilent IO Libraries Suite 14.1 also supports third-party 488.2-compatible adapters through the Agilent SICL I/O API.  So when VEE queries both SICL and 488.2 for available GPIB adapters, it finds the NI GPIB adapter twice.  VEE cannot tell that the two I/O API's adapter references are referring to the same physical adapter. 

You could even see this behavior with Agilent GPIB adapters if you modify the 488.2 board number so that it is in the low single digits (about 0 - 3).  Agilent VEE Pro only searches for 488.2-compatible GPIB interfaces that have board numbers in the low single digits.  The Agilent IO Libraries Suite assigns Agilent GPIB adapters a 488.2 board number starting with 10, so VEE does not "see" Agilent GPIB boards through 488.2 by default, only through SICL. 

The only problem these multiple copies cause is user confusion.  You can delete the extra copy of the adapter in the VEE instrument manager to reduce the confusion.  Unfortunately, every time you search for all instruments in the instrument manager you will have to delete the spare interface again.

If it is absolutely essential to stop this behavior for an Agilent GPIB interface you can increase its 488.2 board # outside of the Agilent VEE Pro board search range.  If it is a National Instruments GPIB interface you can delete the interface in the Agilent Connection Expert and turn off the automatic discovery of I/O resources feature in the Options dialog box of the Agilent Connection Expert so the interface does not get re-configured the next time you use ACE.  You may think that right-clicking an NI GPIB adapter in ACE and choosing the "Ignore" option would work but this only works for Agilent VISA, not SICL.

Regards,

Robin Irwin


---------------------------------------------------------
Applications Engineer
Marketing Dept.
Wireless Division

Telnet  : 313 5429
Direct   : +44 131 335 7429
FAX     : +44 131 335 7229
Email    : robin_irwin@agilent.com
---------------------------------------------------------
www.agilent.com/find/N4010A
www.agilent.com/find/N4010A_zigbee
---------------------------------------------------------

-----Original Message-----
From: Daly, Denis [mailto:dalyd@tycoelectronics.com]
Sent: 22 November 2005 12:08
To: VRF
Subject: RE: [vrf] VEE and Suite 14 IO Libraries Installation problem/ w2k versus X P / IOSuite14.1 Bug ?

Hi All,

We have also had trouble after installing Suite 14 and 7.51, with NI Card.

Agilent's Intuilink stopped functioning! We were attempting to download the screen image from an E4406A VSA. Our fix was to uninstall 7.51 and Suite 14 and simply use 7.0 and M01.01.04 I/O.

Also we have noticed that when Suite 14 searches the GPIB bus it often returns more instruments than actually exist. We are concerned enough that we have delayed installing VEE 7.51 and Suite 14 onto our machines.

Denis

P.s. Have Agilent any possible explanation for these issues?

-----Original Message-----
From: Gregg Levine [mailto:gregg.drwho8@gmail.com]
Sent: 22 November 2005 11:30
To: VRF
Cc: VRF
Subject: Re: [vrf] VEE and Suite 14 IO Libraries Installation problem/ w2k versus X P / IOSuite14.1 Bug ?

Hello from Gregg C Levine
Detlef, I'm not one to disagree with you, even today. But that's not the case. I went to the page you cited, and it turns out that they do accept attachments. Scroll down to the entire form and there you'll find places to place everything. They want in a few different places everything you can think of, plus a few obvious. Like for example the host machine is running a release of Win2K, plus what service pack number, release of VEE, et cetera. Plus everything else that you can think of.
--
Gregg C Levine gregg.drwho8@gmail.com
"This signature was once found posting rude  messages in English in the Moscow subway."


On 11/22/05, Baranski, Detlef <Detlef.Baranski@pilkington.de> wrote:
>
>
> Okay, like in the past, the agilent defect from at:
>
> http://adn.tm.agilent.com/index.cgi?CONTENT_ID=881
>
> did not accept my attachments...
> so I hope it will reach you via the vrf mail.
>
> Perhaps its better to install a BUG Mail address ?
>
>
> detlef
>
>
> -----Ursprngliche Nachricht-----
> Von: Baranski, Detlef
> [mailto:Detlef.Baranski@pilkington.de]
> Gesendet: Dienstag, 22. November 2005 10:59
> An: VRF
> Betreff: [vrf] VEE and Suite 14 IO Libraries Installation problem/ w2k
> versus X P / IOSuite14.1 Bug ?
>
>
> I got the following problem now:
>
> System win2k SP4.
> After installing suite 14.1 and then Agilent Vee 7.51, I got these
> messages when I try to run Find Instruments  in the instrument manager
> after loading a old program: see pictures.
>
> If I run an empty vee file, no problem.
>
> On a WinXP SP2 machine- no problem with this.
>
> I am going to send this to the bug report form. As I think it is a bug ?
>
> Any suggestions ?
>
> Thanks,
> detlef
>
>
>
> -----Ursprngliche Nachricht-----
> Von: IRWIN,ROBIN (A-Scotland,ex1) [mailto:robin_irwin@agilent.com]
> Gesendet: Dienstag, 8. November 2005 18:04
> An: VRF
> Betreff: RE: [vrf] VEE and Suite 14 IO Libraries Installation problem
>
> I've also got concerns over IO suite 14.1 and NI. I am trying to find
> out more about what the problems might be...
>
> Regards,
>
> Robin Irwin
>
>
> ---------------------------------------------------------
> Applications Engineer
> Marketing Dept.
> Wireless Division
>
> Telnet  : 313 5429
> Direct   : +44 131 335 7429
> FAX     : +44 131 335 7229
> Email    : robin_irwin@agilent.com
> ---------------------------------------------------------
> www.agilent.com/find/N4010A
> www.agilent.com/find/N4010A_zigbee
> ---------------------------------------------------------
>
>
> -----Original Message-----
> From: Baranski, Detlef
> [mailto:Detlef.Baranski@pilkington.de]
> Sent: 08 November 2005 15:55
> To: VRF
> Subject: AW: [vrf] VEE and Suite 14 IO Libraries Installation problem
>
> Any News in this item ?
> I want to install 14.1 with 7.51 and a NI-PCMCIA GPIB Card.
> Should I not do that ?
>
> Best regards,
> detlef
>
>
>
>
>
>
>
>
>
> Von: PURTELL,MICHAEL (A-Sonoma,ex1)
> [mailto:michael_purtell@agilent.com]
> Gesendet: Freitag, 30. September 2005 15:37
> An: VRF
> Betreff: RE: [vrf] VEE and Suite 14 IO Libraries Installation problem
>
> For what it's worth, I experienced the same problem a month ago and
> just to get back in productive mode, had to uninstall vee 7.51 and the
> IO libs version 14.1. I'm currently back to Vee 6.01 and only the
> latest NI drivers
> - no Agilent IO libs. I have an NI PCI-GPIB card installed.
>
> Rumor has it there's a patch for IO libs 14.1? but I haven't had time
> to reinstall everything and try the patch.  We have tons of pre vee 7
> code we use in our lab and need to upgrade everything to 7 but are
> holding until a solution is found. We need to be able to function with
> both versions installed and functioning properly.
>
> Our symptoms after vee 7.51 & io Libs 14.1 - Direct IO can talk once
> or a couple of times and then hang err 811. No more comm.. until the
> program is closed and re-started, where it will talk one or more times
> and then hang again err 811.
>
> Please stay on this because we have some Vee 7 only programming
> requirements in the very near future.
>
> Mike
>
> -----Original Message-----
> From: Martin.C.Lim@nokia.com [mailto:Martin.C.Lim@nokia.com]
> Sent: Thursday, September 29, 2005 1:25 PM
> To: VRF
> Subject: [vrf] VEE and Suite 14 IO Libraries Installation problem
>
> Hello,
>
> Have some issues with VEE 7.0 installation.  Finally upgraded my
> VEE5.0 (yeah I know old) to VEE 7.0.  Installation says I/O Libraries
> 01.01.04 or higher has to be installed.  Didn't have the disk with me. 
> So installed IO Libraries Suite 14 from Agilent's web page.Looked like
> an improved version of IO Libraries.  Installation also uninstalled my M01.00 IO Libraries.
>
> Started my program and I can't talk to any GPIB instrument.  Get VEE
> Run Time Error Error number:811.  Typically I see this only if the
> instrument is off or disconnected.
>
> _System_
> *) VEE5.0 w/ VEE 7.0 installed on top
> *) Suite 14.
> *) NI GPIB card
>
> When I search for instruments in NI Max, I can see them.  I can talk
> to the instruments.  When I start Suite14 it works as well.  But VEE
> can not talk to any instruments.
>
> Is Suite 14 the same as IO Libraries?  As I understand it, VEE7.5
> requires Suite 14.  What am I missing?
>
> Next step is to uninstall Suite 14 and then reinstall IO Libraries
> M01.01.04 from my CD.  Should I try anythign else?  Suite 14 does not
> have an uninstall in "Add/Remove Programs"
>
> martin
>
>
>
>
>
> ---
> You are currently subscribed to vrf as: Detlef.Baranski@pilkington.de
> To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
> To unsubscribe send a blank email to
> "leave-vrf@it.lists.it.agilent.com".
> To send messages to this mailing list,  email "vrf@agilent.com".
> If you need help with the mailing list send a message to
> "owner-vrf@it.lists.it.agilent.com".
> Search the "unofficial vrf archive" at "www.oswegosw.com/vrf_archive/".
> ---
>
> You are currently subscribed to vrf as: gregg.drwho8@gmail.com To
> subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
> To unsubscribe send a blank email to
> "leave-vrf@it.lists.it.agilent.com".
> To send messages to this mailing list, email "vrf@agilent.com".
> If you need help with the mailing list send a message to
> "owner-vrf@it.lists.it.agilent.com".
> Search the "unofficial vrf archive" at "www.oswegosw.com/vrf_archive/".

---
You are currently subscribed to vrf as: dalyd@tycoelectronics.com To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "www.oswegosw.com/vrf_archive/".

---
You are currently subscribed to vrf as: robin_irwin@agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "www.oswegosw.com/vrf_archive/".

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "www.oswegosw.com/vrf_archive/".

Outcomes