AnsweredAssumed Answered

custom menus

Question asked by VRFuser on Jun 18, 2001
Richard,

I managed to do this with no problems.  I made a .mnu file with the
following text:

"MENU->Help"
("Tryout"
  ("Int32"
     [visibleWhen notRunning]
     getDevicesFrom: "c:vee_userMyMenuTryout_Int32.vee"
     [desc "Tryout for vrf question"]
  )
)

... then create the Tryout_Int32.vee file, which is a VEE file containing
nothing but an Int32 object.

The .mnu file must be in the VEE installation directory.  Also, you have to
quit VEE and restart before you see any changes.

Works fine.

Yours,
Warren Pickles



-----Original Message-----
From: RWalker@GeneralMicrowave.com [mailto:RWalker@GeneralMicrowave.com]
Sent: 18 June 2001 13:48
To: vrf@lvld.agilent.com
Subject: vrf: custom menus


Fellow Users,
          I have spent some time working with custom menus for VEE Pro
6.01. I have not been able to add some of the custom objects such as Int32,
Real32. Any additional information other than that which is supplied with
VEE Pro 6.0 would be greatly appreciated.



Richard A. Walker
Test Engineer

Herley Farmingdale
425 Smith Street
Farmingdale, N.Y. 11735-1198

Direct Voice: (631) 630-2086
Main Voice: (631) 630-2000 X286
Fax: (631) 630-2066
mailto: RWalker@GeneralMicrowave.com <mailto:RWalker@GeneralMicrowave.com>
http://www.generalmicrowave.com/ <http://www.generalmicrowave.com/>


---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

Outcomes