AnsweredAssumed Answered

vrf USB support

Question asked by VRFuser on Jul 16, 2007
Latest reply on Jul 16, 2007 by VRFuser
Guys,

 

I posted something on here before about vee support for USB devices, but I never fully got to the bottom of it. Basically, we were evaluating a power head from Rhode and Schwarz. Now we have a Anritsu Spectrum Analyser and we can’t get it to work via USB either.

 

All the custom application software will talk to the instruments fine, so it’s not a hardware problem. We just cannot address it through Vee 7.5. Neither Vee nor VISA will ‘discover’ the USB instrument, in the way that plugging in a new GPIB instrument is discovered. It just won’t see it. We tried the latest NI and Agilent VISA utilities but to no avail.

 

I think I need to get it working through VISA first right? Be it Agilent or NI, if these can’t see it then Vee never will, if I understand it right.

 

I have been into Agilent connection expert and gone into the USB interface properties:

 

USB0

SICL:usb0

Logical unit:20

 

I have tried refreshing the USB bus but it never finds anything on it. If I try to add anything manually it tells me I cannot do it:

 

USB0, status unavailable. Manual adding not supported.

 

When I tried the help it states that you cannot manually add to this interface type and that I must use the refresh here. But the refresh does not pick anything up on the USB interface.

 

What do I need to do to get NI or Agilent VISA to ‘see’ what’s on the USB interfaces? I have tried this on two pc’s running XP home.

 

Thanks,

Nick

 

++++++++++++++++++

Nick Smith

Mirics Semiconductor Inc.

Oakmere, Barley Way

Fleet, Hampshire GU51 2UT

+44 1252 612888 (office)

+44 7863 119699 (mobile)

nick.smithHYPERLINK "mailto:nick.smith@mirics.com"@mirics.com

http://www.mirics.com

++++++++++++++++++

 

 


---
You are currently subscribed to vrf as: hua_jing@agilent.com
To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive".
Search the Agilent vrf archive at "http://vee.engineering.agilent.com".


No virus found in this outgoing message.
Checked by AVG Free Edition.
Version: 7.5.476 / Virus Database: 269.10.6/902 - Release Date: 15/07/2007 14:21

Outcomes