AnsweredAssumed Answered

vrf pid control with hp3252A and VEE

Question asked by VRFuser on Apr 15, 2005
Hi,

I'm trying to set up a PID control of liquid temperature using AgilentVEE and HP 3852A Data Acquisition/Control Unit wich is an old productof HP.
I've looked at the example about using PID, but how can I make comunicate VEE with 3852?

And can I use the high speed voltmeter and the DAC of 3852 for this?
I think, but i did't figure out how.

Thanks!

Berneanu Vicentiu
---You are currently subscribed to vrf as: rsb@soco.agilent.comTo subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".To send messages to this mailing list,  email "vrf@agilent.com".  If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".  

Outcomes