AnsweredAssumed Answered

AW: vrf ActiveX Spreadsheet object

Question asked by detlef.baranski on Nov 15, 2005
Perhaps shorter answer is:

Have a look for examples/excelLibrary/SendingData/DataToCells2D.vee   as an
example without all activex parts...to solve your problem

Via the Vee _Help_Open Examples menue...#

Best regards,
detlef


-----Ursprngliche Nachricht-----
Von: Baranski, Detlef
Gesendet: Dienstag, 15. November 2005 18:36
An: 'Andie Hioki'; VRF
Betreff: AW: [vrf] ActiveX Spreadsheet object

Andie,
with VEE 7.5 you also get the excel - library support. So normally you do
not need these ActixeX -stuff anymore.
Just use the lego blocks from the VEE -Excel menue and voila
To understand how it works have a look for the excel examples. It is much
easier than the activ-x stuff.
Just in case you need more complex scripts, have a look for the example how
you can run the excel macros directly from excel.
So at the end there is really no need for actveX-Excel calls anymore since
vee7.5 - beside the fact you want to use old written code ....

So at the end you have the choice to use both ...but take care of mixing it
.

Best regards,
detlef

-----Ursprngliche Nachricht-----
Von: Andie Hioki [mailto:andie_hioki@sbcglobal.net]
Gesendet: Dienstag, 15. November 2005 08:12
An: VRF
Betreff: [vrf] ActiveX Spreadsheet object

Hello,

I'm new to VEE 7.5. Can anyone tell me how to
access/refer to an ActiveX Spreadsheet object's
cells? I want to be able to assign some values to
the spreadsheet object's cells. All I know right
now is that I have to use a formula and refer to
the spreadsheet object's name. Thank you.

Regards,
Andie



---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "www.oswegosw.com/vrf_archive/".

Outcomes