AnsweredAssumed Answered

vrf Vee 7.5 Dot Net using labels in user functions with event handlers?

Question asked by qigao Employee on Sep 21, 2005
Latest reply on Sep 21, 2005 by qigao
<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.0 Transitional//EN"><HTML><HEAD><META HTTP-EQUIV="Content-Type" CONTENT="text/html; charset=iso-8859-1"><META content="MSHTML 6.00.2900.2722" name=GENERATOR></HEAD><BODY><DIV><FONT face=Arial size=2><SPAN class=018230320-22092005>Is it possible to preposition the markers of a XY Trace?</SPAN></FONT></DIV><DIV><FONT face=Arial size=2><SPAN class=018230320-22092005>I have a program where the operator manually places the markers on the XY Trace then hits a button that does some calculations based on the position of the of the markers. </SPAN></FONT><FONT face=Arial size=2><SPAN class=018230320-22092005>The XY Trace is redisplayed but the markers reappear in a default position. Is it possible to have the markers appear in the same location the operator placed them prior to the redisplay of the trace?</SPAN></FONT></DIV><DIV><FONT face=Arial size=2><SPAN class=018230320-22092005></SPAN></FONT> </DIV><DIV><FONT face=Arial size=2><SPAN class=018230320-22092005></SPAN></FONT> </DIV><DIV><FONT face=Arial size=2><SPAN class=018230320-22092005>John</SPAN></FONT></DIV><BR>---<BR>You are currently subscribed to vrf as: rsb@soco.agilent.com<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list,  email "vrf@agilent.com".  <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".<BR>Search the "unofficial vrf archive" at "www.oswegosw.com/vrf_archive/".</BODY></HTML>  

Outcomes