AnsweredAssumed Answered

AW: vrf Excel

Question asked by detlef.baranski on Dec 14, 2005
Latest reply on Apr 24, 2008 by VRFuser
Belonging the print preview: Save it as a picture in a format like :
Bitmaps (*.BMP) JPEG (*.JPG) Windows Meta File (*.WMF)  GIF87a (*.GIF)
GIF89 (*.GIF) Portable Network Graphics (*.PNG)

you want and illustrate it in Vee via

-----Ursprngliche Nachricht-----
Von: Andie Hioki [mailto:andie_hioki@sbcglobal.net]
Gesendet: Donnerstag, 15. Dezember 2005 09:05
An: VRF
Betreff: [vrf] Excel

Hello,

I'm using VEE 7.5's Excel library/menu, which is a lot easier to use than
ActiveX objects. But I found out that if I have more than one Excel file
open, or if the file that I want VEE to open is already open, then when the
program runs, it runs in the background. It reads from and writes to the
cells just fine, but it hides behind the VEE program.

On the other hand, Excel does run in the foreground if the desired file was
not already opened. But the problem with this case is that it obscures the
pop-up message box to the operator and you can't tell that the program is
waiting for a user response; And vice versa when you click on VEE to answer
the pop-up message, Excel is obscured.

So, is there a way (without using ActiveX) to have the defined print area in
Excel (or the print preview) be added to the user panel? The reason for
this is so the operator can verify the data quickly. Thanks in advance f or
any suggestions.

Regards,
Andie
--- You are currently subscribed to vrf as: Detlef.Baranski@pilkington.de To
subscribe send a blank email to "join-vrf@it.lists.it.agilent.com". To
unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com". To
send messages to this mailing list, email "vrf@agilent.com". If you need
help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com". Search the "unofficial vrf archive" at
"www.oswegosw.com/vrf_archive/".

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "www.oswegosw.com/vrf_archive/".

Outcomes