I just got a HP11713A ATTENUATOR/SWITCH DRIVER and 2 programmable step attenuators (
8494H and 8496H )
I can use direct i/o and send those strings of charactors such as "A12B5678" and get the
attenuator pads to switch on/off.
Q: Is there an instrument driver for this so that you can send a decimal number, like
63, and have the attenuoator re-configured for 63dB?
-dan k.
san diego
Dan K.
'92 Grey Dak CC, 318, 4x2, 46RH, 3.55 rear, 235/75R15, PS, PW, PB, PL, AC.
Mods: Cool air, K&N oil/air, 180* T-Stat, Autolite 3924s, re-located IAT, Trans-Go shift kit.
Future: Swap motor for a slightly modified Magnum 5.9L engine.
__________________________________
Yahoo! Mail - PC Magazine Editors' Choice 2005
http://mail.yahoo.com
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "www.oswegosw.com/vrf_archive/".
Search the "unofficial vrf archive" at "www.oswegosw.com/vrf_archive/".