AnsweredAssumed Answered

Re2: vrf matlab function

Question asked by rsb on Dec 8, 2005
Stan Bischof (Richard S) <rsb@soco.agilent.com> wrote:
> arief12 <arief12@netvision.net.il> wrote:
> > Hi all
> >
> > I'm trying to use matlab function "taxtscan" and it seems that vee doesn't
> > recognize it, and show me an error.
> >
> > I would like to know if someone has used this function.
> >
> > There are build in matlab function in vee, what about function that doesn't
> > in the list, does vee know to work with them too?
>
> VEE comes with an OEM version of Matlab, which by itself
> will execute a huge array of Matlab functions- but not everything.
> If the function exists in some toolbox in Matlab that doesn't
> come with this OEM version, then you can still use it from VEE,
> BUT you need to install a standalone Matlab with that toolbox.
>
> Then VEE will interface to your standalone Matlab rather
> than the OEM Matlab.

Did a little poking and I'll assume that "taxtscan" is a typo
and you really meant "textscan", in which case there may be
a problem. So far as I can tell "textscan" was added to Matlab
for rev 7. VEE 7.x ships with OEM rev 6.

So unless the VEE interface will talk to Matlab 7 ( no idea
but maybe VEE folks will chime in with the answer ) then
you won;t be able to use "textscan" in a Matlab Script object
even if you do buy Matlab. In current versions of VEE at least.

regards

Stan


--------------------------------------------------------------------------
Stan Bischof  Agilent Technologies  707-577-3994  stan_bischof@agilent.com
--------------------------------------------------------------------------

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "www.oswegosw.com/vrf_archive/".

Outcomes