AnsweredAssumed Answered

vrf Remote Channel Display

Question asked by fukui.yutaka on Jan 5, 2005
Hi,


Use "CHAN N" command!

The following examples are from "N3300A, - N3307A DC Electronic

Loads Programming Guide" obtained from Agilent's Home Page.


---------------------------------------------------------------------------------------------------------
CC Mode Example
This example selects channel 1, sets the current level to 1.25 A and
reads back the actual current value.
10 OUTPUT 705; "CHAN 1"
20 OUTPUT 705;"INPUT OFF"
30 OUTPUT 705;"FUNC CURR"
40 OUTPUT 705;"CURR:RANG MIN"
50 OUTPUT 705;"CURR 1.25"
60 OUTPUT 705;"INPUT ON"
70 OUTPUT 705;"MEAS:CURR?"
80 ENTER 705;A
90 DISP A
100 END
Line 10: Selects the channel 1 module.
Line 20: Turns off the input.
Line 30: Selects the CC mode.
Line 40: Selects the low current range.
Line 50: Sets the current level to 1.25 amps.
Line 60: Turns on the input.
Line 70: Measures the actual input current and stores it in a buffer
inside the electronic load.
Line 80: Reads the input current value into variable A in the computer.
Line 90: Displays the measured current value on the computer's display.

CV Mode Example
This example selects channel 2, presets the voltage level to 10 volts,
and selects the external trigger
source. When the external trigger signal is received, the channel 2 CV
level will be set to 10 volts.
10 OUTPUT 705; "CHAN 2;:INPUT OFF"
20 OUTPUT 705;"FUNC VOLT"
30 OUTPUT 705;"VOLT 0"
40 OUTPUT 705;"VOLT:TRIG 10"
50 OUTPUT 705;"TRIG:SOUR EXT"
60 OUTPUT 705;"INPUT ON"
70 END
Line 10: Selects channel 2 and turns off the input.
Line 20: Selects the CV mode.
Line 30: Sets the initial voltage level to 0 volts.
Line 40: Sets the triggered voltage level to 10 volts.
Line 50: Selects the external input as the trigger source.
Line 60: Turns on the channel 2 input.
---------------------------------------------------------------------------------------------------------

Regards,
FUKUI Yutaka

> "Carver, John" wrote:
>
> Is there a SCPI command or a remote way to change the display on a
> 6050A or N3300A electronic load?  I am trying to remotely change the
> display of the load from channel 1 to another channel.  The only way I
> have now is to place the load back into local mode than manually
> change the display via the front panel.  Thank you.
>
>      John D. Carver
>      Test Technician
>      Product Reliability Center
>      Global Automotive Division, America's North
>      _______________________________________________
>      Tyco Electronics
>
>      3800 Reidsville Road            Phone:  336-727-5805
>      Winston Salem, NC  27101-2166   Fax:    336-727-5153
>      Mail Stop: 079-050              Email:
>      john_carver@tycoelectronics.com
>
>
> ---
> You are currently subscribed to vrf as: fukui.yutaka@jp.fujitsu.com
> To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
> To unsubscribe send a blank email to
> "leave-vrf@it.lists.it.agilent.com".
> To send messages to this mailing list, email "vrf@agilent.com".
> If you need help with the mailing list send a message to
> "owner-vrf@it.lists.it.agilent.com".

--
*****************************************************************
*  $BJ!0f!!K-!J (BFUKUI Yutaka)
* E-Mail: fukui.yutaka@jp.fujitsu.com
*  $BIY;NDL3t<02q<R!!@n:j9)>l (B
*  $B$b$N$E$/$j?d?JKIt!&@8;:5;=Q3+H/E}3gIt!!;n835;=Q (BPj <-- 2004/10/01 $B$h$j (B
$B?&@)$,JQ$j$^$7$? (B
*  $B7WB,@_Hw3+H/It (BHomePage http://www.psl.fujitsu.co.jp/htd2/ksk/
*  $B@n:j;TCf866h>e>.EDCf#4 (B- $B#1 (B- $B#1!!M9JXHV9f!' (B211-8588
* TEL  $B!!30@~ (B 044-754-3661, $B!!Fb@~ (B 711-3-1966,7 <-- 2004/09/27 $B$h$j30@~$,JQ (B
$B$j$^$7$? (B
* FAX  $B!!30@~ (B 044-754-3509, $B!!Fb@~ (B 711-3-5359
*****************************************************************

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes