Thanks Shawn. I just found out that this isn't going to work the way that
I had hoped. As it turns out, Tek has developed their own version of VISA,
based off of the NI VISA. And their VISA will not work with anything else
but that software package.
Thanks again, and now off to plan B. I may end up having to use VEE to
pull all of the data from the scopes and save them into a text or CSV file.
Thanks for the help.
Tom
|---------+---------------------------->
| | "Shawn Fessenden"|
| | <shawn@testech-lt|
| | d.com> |
| | |
| | 03/18/2005 09:58 |
| | AM |
| | |
|---------+---------------------------->
>------------------------------------------------------------------------------------------------------------------------------|
| |
| To: <Thomas.Mitchell@Autoliv.com>, "'VRF'" <vrf@agilent.com> |
| cc: |
| Subject: RE: [vrf] VEE & Tektronix Wavestar software |
>------------------------------------------------------------------------------------------------------------------------------|
> i saw some examples a few weeks ago that used VEE
> to control other programs.
The best way to control other applications is to use it's exposed
Automation
interface, but not all applications expose an Automation interface.
The sure-fire will-handle-almost-anything way is to use SendKeys. As long
as
the programs you want to control provide hotkeys, keyboard accelerators or
the fields & buttons you want to interact with are reachable using the Tab
key, you can use SendKeys.
The SendKeys method is implemented by almost any VB or VBA library - for
instance the Word or Excel Application objects or the Scripting library.
You
can find the classic SendKeys example at http://www.preciselyso.co.uk in
"Tools & Tips" or in the VRF Archive - search attachments for SendKeys.
-SHAWN-
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
> to control other programs.
The best way to control other applications is to use it's exposed Automation
interface, but not all applications expose an Automation interface.
The sure-fire will-handle-almost-anything way is to use SendKeys. As long as
the programs you want to control provide hotkeys, keyboard accelerators or
the fields & buttons you want to interact with are reachable using the Tab
key, you can use SendKeys.
The SendKeys method is implemented by almost any VB or VBA library - for
instance the Word or Excel Application objects or the Scripting library. You
can find the classic SendKeys example at http://www.preciselyso.co.uk in
"Tools & Tips" or in the VRF Archive - search attachments for SendKeys.
-SHAWN-
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".