<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.0 Transitional//EN"><HTML><HEAD><META HTTP-EQUIV="Content-Type" CONTENT="text/html; charset=iso-8859-1"><META content="MSHTML 6.00.2800.1479" name=GENERATOR></HEAD><BODY><DIV><FONT face=Arial size=2><SPAN class=179305615-01022005>Hello,</SPAN></FONT></DIV><DIV><FONT face=Arial size=2><SPAN class=179305615-01022005></SPAN></FONT> </DIV><DIV><FONT face=Arial size=2><SPAN class=179305615-01022005>I want to convert at string containing a hex value to a decimal value.</SPAN></FONT></DIV><DIV><FONT face=Arial size=2><SPAN class=179305615-01022005>Is there another way to do that than the "From string" ?</SPAN></FONT></DIV><DIV><FONT face=Arial size=2><SPAN class=179305615-01022005></SPAN></FONT> </DIV><DIV><FONT face=Arial size=2><SPAN class=179305615-01022005>I have been looking in the Function & Object browser, but I couldn't find anything.</SPAN></FONT></DIV><DIV><FONT face=Arial size=2><SPAN class=179305615-01022005></SPAN></FONT> </DIV><DIV><FONT face=Arial size=2><SPAN class=179305615-01022005>Br,</SPAN></FONT></DIV><DIV><FONT face=Arial size=2><SPAN class=179305615-01022005>Susanne Jrgensen</SPAN></FONT></DIV>---<BR>You are currently subscribed to vrf as: rsb@soco.agilent.com<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list, email "vrf@agilent.com". <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".</BODY></HTML>
I like to be advised if you have an example of VeePro code for data
acquisition from PNA Network Analyzer N5230A. Thanks.
zs
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".