AnsweredAssumed Answered

vrf AW: 8753 Programmers Reference....and program examples

Question asked by detlef.baranski on Feb 2, 2005
VRF,

I am having problems communicating to a micro through VEE 7.

I found that sending a text string to the micro and reading the micro's
buffer shows some of data is not received--almost every other character is
dropped.

If I send a single character to the micro--sometimes the micro does not see
it.

Receiving data from the micro yields 100% data transfer through VEE.

I can use XP's Hyperterm with success in both transmit and receive modes.

Communication parameters are 19200, No Parity, 1 Stop Bit and no Handshake.

I am confused why Hyperterm works and VEE is falling short.

Any help would be greatly appreciated.

Thanks in advance...

Harry Kubiak



---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes