AnsweredAssumed Answered

vrf Matlab: Adding Ouput causes Error 405

Question asked by rsb on Jun 3, 2005

> Hi
>
> here is a neat trick:
> Vee seems to loose formulas in matlab script boxes.
> This is why I get error 405!
>
> Please check out the attached screen shots:
> file 1 is a screen shot of the test script which contains the A=123;
> line
> as I had it when trying out the code.
> I then saved it and reloaded it and over sudden the A=123; is gone!
>
> If that's not a bug I don't know
>
> Maybe it has to do with the fact that I have Vee 6, Vee 7 and Vee 7.5
> installed???


Which version of VEE are you doing that work on?

Stan

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes