AnsweredAssumed Answered

vrf Direct I/O Command to DCA 86100A Osci

Question asked by VRFuser on May 9, 2003
"Schlieker, Reiner" <reiner.schlieker@siemens.com> wrote:
> I noticed in the example that the To String - Case object was still
> retrieving values from the array.  I wonder if it would be faster if the
> text was imbedded in the To String...?
>
> Reiner

Actually slows it down marginally. See below.

Also, since you can do most anything with a formula, I've included
another method that may be of use. It is arguably more elegant since
it is a single object, though is also perhaps more obscure.

Stan

Outcomes