AnsweredAssumed Answered

AW: vrf detection of max and min in a signal/ Zero Crossings

Question asked by detlef.baranski on Aug 11, 2005
> It is the kind that appear in the program explorer

Sorry, I should have been more specific. If you post the header file
(something.h, probably in the board installation's include or example
directory) for the compiled functions I can probably translate them into VEE
parsable definitions for you. Compound types (if any) will probably cause
you headaches. These are identified by "struct" or "typedef struct". They
can be handled by VEE's CFI, but they tend to be a little scary.
-SHAWN-



---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes