AnsweredAssumed Answered

AW: vrf VEE and USB

Question asked by detlef.baranski on Apr 5, 2005
Latest reply on Apr 5, 2005 by detlef.baranski
There is a USB controler solution under :
http://www.my-vee.de/download.html


which is named: USB Steuerung in VEE

It s a nice example also for elder VEE Versions.
If you need a translation of the german description, let me know.

best regards,
detlef



-----Ursprngliche Nachricht-----
Von: Gregg C Levine [mailto:landocalrissian@att.net]
Gesendet: Montag, 4. April 2005 18:45
An: VRF
Betreff: [vrf] VEE and USB


Hello from Gregg C Levine
Would someone please correct my assertions if I've erred any. I've made the
attempt to err on the side of caution.
VEE uses only the subset of the USB features that correspond to the T&M
devices that the company has created. (See matrix on their site for
references.)

To use an HID such as a Microchip based solution would require the use of a
custom DLL library, and accessabilty header file. (Or not, if it was written
as an Active X type library.

For those of you who know me reasonably well by now, this is the time of
year when I get innundated with new project ideas, some of them customer
ones. This one, and the previous message regarding the Peek and Poke library
are actually mine.
This message and any attachments are confidential, for the exclusive use of
the addressee and may be legally privileged. Any other distribution, use or
reproduction is unauthorised and prohibited. If you have received this
message in error, please notify the sender immediately and delete the
message from your system.

Visit our internet site at http://www.pilkington.com

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes