AnsweredAssumed Answered

vrf MultiFrameScan with more than one backloadabel tunable laser

Question asked by VRFuser on Jun 27, 2005
<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.0 Transitional//EN"><HTML><HEAD><META http-equiv=Content-Type content="text/html; charset=us-ascii"><META content="MSHTML 6.00.2800.1505" name=GENERATOR></HEAD><BODY><DIV><FONT face=Arial size=2><SPAN class=006182114-27062005>Hello members,</SPAN></FONT></DIV><DIV><FONT face=Arial size=2><SPAN class=006182114-27062005></SPAN></FONT> </DIV><DIV><FONT face=Arial size=2><SPAN class=006182114-27062005>That is my first contact to the "Agilent VEE VRF Discussion Forum". </SPAN></FONT></DIV><DIV><FONT face=Arial size=2><SPAN class=006182114-27062005>My problem is to measure optical filters with 3 agilent TLS in 3 seperate 8164A mainframes (81600B-200;81600B-140;81600B-130) and one agilent powermeter and a agilent switch1x4 in a seperate mainframe (a HP81634 powermeter and a HP81595A in a 8163A mainframe). I connect the 3 TLS-outputs to the switch and from the switch com-port to the powermeter. Now i want to measure with the agilent plug&play driver, but for use the plug&play driver i must connect the TLS-trigger-output to the powermeter mainframe trigger-input. When i connect 2 TLS trigger- outputs with the powermeter mainframe-trigger-input it works.</SPAN></FONT></DIV><DIV><FONT face=Arial size=2><SPAN class=006182114-27062005>When i connect the third TLS trigger-output to the triggerbus it doesnt work and i got the error message "No trigger writing Check trigger connection". What can i do??</SPAN></FONT></DIV><DIV><FONT face=Arial size=2><SPAN class=006182114-27062005></SPAN></FONT> </DIV><DIV><FONT face=Arial size=2><SPAN class=006182114-27062005></SPAN></FONT> </DIV><DIV><FONT face=Arial size=2><SPAN class=006182114-27062005>PS.: the normal MultiFrameScan-connection is one TLS and many powermeters but i need 3 TLS and one powermeter to scan with the first TLS then with the second TLS and then with the third TLS. To get the hole filtercurve.</SPAN></FONT></DIV><DIV><FONT face=Arial size=2><SPAN class=006182114-27062005></SPAN></FONT> </DIV><DIV><FONT face=Arial size=2><SPAN class=006182114-27062005>best regards</SPAN></FONT></DIV><DIV><FONT face=Arial size=2><SPAN class=006182114-27062005></SPAN></FONT> </DIV><DIV><FONT face=Arial size=2><SPAN class=006182114-27062005>Tino</SPAN></FONT></DIV><BR>---<BR>You are currently subscribed to vrf as: rsb@soco.agilent.com<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list,  email "vrf@agilent.com".  <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".</BODY></HTML>  

Outcomes