<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.0 Transitional//EN"><HTML><HEAD><META http-equiv=Content-Type content="text/html; charset=us-ascii"><META content="MSHTML 6.00.2800.1498" name=GENERATOR></HEAD><BODY><DIV dir=ltr align=left><FONT face=Arial color=#0000ff size=2><SPAN class=876304015-24062005>Rob </SPAN></FONT></DIV><DIV dir=ltr align=left><FONT face=Arial color=#0000ff size=2><SPAN class=876304015-24062005>Are you doing an "Execute Close" on com2 just before your Stop? That might be what's holding the process. I seem to recall having a similar problem once and the Execute Close fixed it.</SPAN></FONT></DIV><DIV dir=ltr align=left><FONT face=Arial color=#0000ff size=2><SPAN class=876304015-24062005>Dave</SPAN></FONT></DIV><BR><DIV class=OutlookMessageHeader lang=en-us dir=ltr align=left><HR tabIndex=-1><FONT face=Tahoma size=2><B>From:</B> Robert A Marquardt [mailto:ramarquardt@ra.rockwell.com] <BR><B>Sent:</B> Thursday, June 23, 2005 7:19 PM<BR><B>To:</B> VRF<BR><B>Cc:</B> vrf@it.lists.it.agilent.com<BR><B>Subject:</B> [vrf] ML1100 Functional tester<BR></FONT><BR></DIV><DIV></DIV><P><FONT face=sans-serif size=2>I found a hanging veerun.exe process in the Task Manager after killing veerun. I can't get rid of it without rebooting.</FONT> <P><FONT face=sans-serif size=2>This occurs when exiting runtime VEE by executing a STOP. However, the STOP is only for one thread. Could it be that my other thread (just monitors F-keys) is the hangup? If so, how do I get both threads to exit?</FONT> <P><FONT face=sans-serif size=2>It grabs com2 and won't let go. So when TEST starts it shows another process owns com2.</FONT> <P><FONT face=sans-serif size=2>Not sure if there is a solution for this or why it happens.</FONT> <P><FONT face=sans-serif size=2>System in Win XP Pro, VEE 7.03</FONT> <P><FONT face=sans-serif size=2>....Rob</FONT> --- You are currently subscribed to vrf as: Dave.Andersen@gdc4s.com To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com". To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com". To send messages to this mailing list, email "vrf@agilent.com". If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".</P><BR>---<BR>You are currently subscribed to vrf as: rsb@soco.agilent.com<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list, email "vrf@agilent.com". <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".</BODY></HTML>
<p><font size=2 face="sans-serif">I found a hanging veerun.exe process in the Task Manager after killing veerun. I can't get rid of it without rebooting.</font>
<p><font size=2 face="sans-serif">This occurs when exiting runtime VEE by executing a STOP. However, the STOP is only for one thread. Could it be that my other thread (just monitors F-keys) is the hangup? If so, how do I get both threads to exit?</font>
<p><font size=2 face="sans-serif">It grabs com2 and won't let go. So when TEST starts it shows another process owns com2.</font>
<p><font size=2 face="sans-serif">Not sure if there is a solution for this or why it happens.</font>
<p><font size=2 face="sans-serif">System in Win XP Pro, VEE 7.03</font>
<p><font size=2 face="sans-serif">....Rob</font>
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".