AnsweredAssumed Answered

vrf IO lib installation

Question asked by VRFuser on Jan 12, 2005
Ok, thought you wanted to toss the VEE.  What I do for simple installs, ( I
don't worry 'bout the size) is to use dotNet.  Make all calls from dotNet
and use the dotnNet framework to package all software and use windows
install.  One CD.  (Yea, yea, I know, Windows is a memory hog, but who you
gonna call?)

In fact, I did one install by dumping the entire design environment, so if
something was not found, like VEERUN, I'd install it from the install
directory,  all automatically without intervention, simply by making sure
everything was in the design environment and debugged.


rufus

-----Original Message-----
From: David Moodie [mailto:d.moodie@optosci.com]
Sent: Thursday, January 13, 2005 5:26 AM
To: VRF
Subject: [vrf] RE: IO lib installation

Hi Rufus

We need a little bit more functionality than Hyper terminal. We are also
using Matlab, within Vee for our analysis, essentially doing a cut down BER
measurement based upon data that is captured from the scope.

We would like to create a neater installation procedure, and with less user
intervention than is required for installing the full runtime version of the
IO libs.

We use RS232 for the data transfer on the basis that it is the lowest common
denominator.

cheers

David

> -----Original Message-----
> From: Rufus Warren [mailto:rwarren@amti.net]
> Sent: 12 January 2005 21:47
> To: 'David Moodie'; 'VRF'
> Subject: RE: [vrf] IO lib installation
>
>
> Not sure if I understand.  If what you want is to read/write to an
> rs232 port and you already have the messages you wish to send/receive,
> then use a HyperTerminal script instead of the VEE.
>
> rufus
>
> -----Original Message-----
> From: David Moodie [mailto:d.moodie@optosci.com]
> Sent: Wednesday, January 12, 2005 11:00 AM
> To: VRF
> Subject: [vrf] IO lib installation
>
>
> We distribute a vee runtime with one of our kits, to allow data to be
> read from a 'scope via the rs232 interface.
> currently we include the full IO libs installation with the runtime
> but ideally we would like to minimise the installed files and make the
> installation run a little more smoothly.
>
> With regard to this does anyone know if it is possible to install only 
> the IO library components necessary to allow use of the rs232 port (or
> a USB
> /rs232 converter)?
>
> cheers
>
> David
>
>
>
> ---
> You are currently subscribed to vrf as: rwarren@amti.net To subscribe
> send a blank email to "join-vrf@it.lists.it.agilent.com".
> To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
> To send messages to this mailing list,  email "vrf@agilent.com".
> If you need help with the mailing list send a message to
> "owner-vrf@it.lists.it.agilent.com".


---
You are currently subscribed to vrf as: rwarren@amti.net To subscribe send a
blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".


---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes