AnsweredAssumed Answered

PNA-X IMD leveling configuration via SCPI

Question asked by andyTPE on Apr 10, 2012
Latest reply on Apr 10, 2012 by andyTPE
Hello PNA-X users,

I am running A.09.42.16 on a PNA-X and trying to configure the power leveling mode via SCPI.

The GUI provides me with 4 options:
1 Set input power
2 Set input power, receiver leveling
3 Set input power, equal tones at output
4 Set output power, receiver leveling

The help file documents:
sense:imd:tpower:equalize:state
sense:imd:tpower:set

I think the latter command, will allow me to set states 1 and 4.  However, if I want to configure for case 2 (set power at the input, but use receiver leveling), is the an undocumented IMD command that I can set.  Or do I have to start programming the receiver leveling system (in which case I suspect I will have to manage which sources I configure the leveling for - rather than letting the firmware team do the hard work!)

If anyone can shed some light on the best way to config this aspect of an IMD measurement, I would be very grateful.

Thanks

Andy  

Outcomes