AnsweredAssumed Answered

vrf Truncated number problem

Question asked by VRFuser on Sep 7, 2006
This one worked great.
 
Thanks for the help everyone,
Kevin


  _____  

From: Iulia Popovici [mailto:iulia.popovici@urbanet.ch]
Sent: Wednesday, September 06, 2006 4:42 PM
To: Reed, Kevin
Subject: Re: [vrf] Truncated number problem


Kevin, try the attached.
 
Regards, Julia
 
 
 
----- Original Message -----
From: "Reed, Kevin" <HYPERLINK "mailto:Kevin.Reed@analog.com"Kevin.Reed@analog.com>
To: "VRF" <HYPERLINK "mailto:vrf@agilent.com"vrf@agilent.com>
Sent: Wednesday, September 06, 2006 5:48 PM
Subject: [vrf] Truncated number problem


Hey everyone,

This seems like it should be a pretty simple thing to fix but I am yet
to find what is making this happen so any help you can extend me would
be greatly appreciated.  So basically I am loading an array of numbers
from a file in binary form.  I have the file to read as an int32, but it
seems that when the number is read and displayed it is only reading the
last 8 bits in the number no matter how many more bits there are. I have
included the snippet of the code that I am working with along with a
text file I am using to experiment with.  If anyone has time to look at
this that would be great.

Thanks for the help again,
Kevin Reed

 <<test.vee>>  <<test.txt>>

 


---

To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "www.oswegosw.com/vrf_archive/".  

Outcomes