AnsweredAssumed Answered

Fw: vrf Scheduled testing

Question asked by yarien on Aug 21, 2006
GAO,QI (A-Sonoma,ex1) wrote the following on 20/08/2006 02:01:
>
> From VEE's online help under Memory leak, it documents two known
> scenarios.
>
> Here is one of them.  Notice the "expected course of program execution".
>

>
> Your program may leak memory when a Formula object uses an Error pin,
> and the Error pin fires during the expected course of program
> execution. An example of this condition is where an expression
> performs a divide-by-zero operation causing the Error pin to fire.
>

>

>
> Here is the other scenario -
>
> The memory leak condition exists only if a transaction object contains
> two READ transactions that both reference the same output pin, but use
> different data types. The following pair of transactions is an example:
>

>
> READ TEXT x STR
>
> READ TEXT x REAL
>
How big is the memory leak in the case of the Error pin leak?  Is it a few k per error, or is it dependent on the type of error?  If it's a small memory leak then I'm not sure I'd see its effects after just five or six iterations of my main program loop.

As for the second memory leak, I don't have any IO that looks like that.  I keep it simple, one type per variable!

Increasing the available swap memory seems to have done the trick, but it seems like a dirty solution.
>
>  --
>
> Graeme Hilton
> R&D Engineer
>
> Schlumberger Sensa
> Gamma House, Enterprise Road,
> Southampton, SO16 7NS
> Tel: 023 8076 5596
> Fax: 023 8076 5501

---
To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "www.oswegosw.com/vrf_archive/".

Outcomes