AnsweredAssumed Answered

Protocol verification using Logic Analyzer (Agilent 16803A)

Question asked by mullish on Apr 26, 2012
Hi ,

I want to know whether I can check the the type of protocol on a pin connected to LA using a C# program.

My setup is as below :

1. The hardware has a program which gererates various protocols like i2c, spi, LIN etc.
2. The pin on which the protocol is generated is connected to LA
3. LA is connected to PC using a GPIB cable.
4. A C# application is running on the PC.

The PC application should show the type of the protocol on pin. I have Agilent 16803A Logic Analyzer.

Can members give pointers to the documents/drivers to do this?

thanks
Mullish  

Outcomes