AnsweredAssumed Answered

N1996 Channel Power Measurement using IVI-COM driver

Question asked by clive.packer on Mar 29, 2012
Latest reply on Apr 6, 2012 by fanfansimon
I'm trying to perform a series of automated channel power measurements using Vee to control a N1996 CSA. I can configure the instrument and make the measurement using the agilentCSAClass.ChannelPower class but I can't see a way to get the actual channel power measurement back from the instrument - the number that's displayed in the lower left of the screen representing the channel power over the integration bandwidth I've configured. I don't want  the whole trace, peak, or anything like that, I just need the one channel power measurement. How can I read this back from the instrument?  

Outcomes