AnsweredAssumed Answered

vrf I'm a new Vee user..trying to connect to a HP34970a

Question asked by VRFuser on Apr 6, 2006
Oh yes, and since you are using RS-232, you need to send a REM command first
to put the instrument in remote or it simply won't accept commands.

Jay Nemeth-Johannes
Smart Sensor Systems
720 SW 14th Street
Loveland, Colorado 80537
(970) 663-0006
www.SmartSensorSystems.com



> -----Original Message-----
> From: Coles, Henry [mailto:henry.coles@hp.com]
> Sent: Thursday, April 06, 2006 6:20 PM
> To: VRF
> Subject: [vrf] I'm a new Vee user..trying to connect to a HP34970a
>
> Hello Vee experts,
>
> I just got Vee 7.51 and I'm in the process of trying to write
> a "driver"
> to get 8 to 10 thermocouple temperatures with say 1 second
> scans from an HP34970a which is a multichannel recorder, I
> guess you could call it.
> Of course I can start by just getting one temperature one
> time.  My thought is that the most common device anyone would
> connect to would be the HP34970a, but that's just a guess.
>
> So far I only have an RS232 connection to the device.  I
> think I need to use Direct I/O to talk to it.  I have
> programming book for the device and have tried to send a
> "*IDN?" or "IDN?" to the device to see if I can get something
> back.  I got a bunch of syntax errors/etc. just entering the
> first Write line.  It does look like Vee sees the device on
> the end of the #1 RS232 port.
>
> It looks like a panel driver can only be used if I have an
> HPIB connection which I don't have and can't quite figure out
> the VXIplug and play.....so I'm down to trying the direct I/O
> approach.
>
> Any help appriciated.  Sorry for the newbee run around.
> Maybe there is a file or old email someone can send me to help out.
>
> Thanks very much in advance.
>
> -Henry
>
> ---
> You are currently subscribed to vrf as:
> jay.johannes@completetest.com To subscribe please send an
> email to: "vrf-request@lists.it.agilent.com" with the word
> subscribe in the message body.
> To unsubscribe send a blank email to
> "leave-vrf@it.lists.it.agilent.com".
> To send messages to this mailing list,  email "vrf@agilent.com".
> If you need help with the mailing list send a message to
> "owner-vrf@it.lists.it.agilent.com".
> Search the "unofficial vrf archive" at
> "www.oswegosw.com/vrf_archive/".
>




---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "www.oswegosw.com/vrf_archive/".

Outcomes